The datasheet for the ADS1291/1292 advises us to "avoid stray wiring capacitance" for sensitive analog signals. It also advises shielding those signals. My instinct is to place the sensitive traces above a ground region tied to AVSS, and also flooding areas adjacent to the traces with AVSS, to minimize signal coupling from other sources. However, the AVSS regions will increase the stray capacitance. How do I resolve this apparent tension? Or is the "stray capacitance" mentioned actually the capacitance to random external nets, and AVSS would therefore be okay to keep close?
I could also include guard rings, if there is an appropriate driven signal available to act as a guard. Not being aware of any, I assumed AVSS would be the signal to keep close to the sensitive signals.
Thanks,
Scott