This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

4Ch video decoder multiplexer

Guru 20755 points

Other Parts Discussed in Thread: TVP5158

Hello,

Are the video decoders (such as tvp5158, etc) support mutliple sources each with different resolution, frame rate, and interlace type (I/P).

For example can I use the following inputs into 4channel video decoder ? 

1. Sensor 1 (CCD) Raw Images 720x704x2 60Hz 60 128K 4
2. Sensor 1 (CCD) Processed Images 640x480x1 30Hz 10 48K 1.5
3. Sensor 2 (FLIR) Raw Images 640x512x2 60Hz 40 128K 4
4. Sensor 2 (FLIR) Processed Images 640x480x1 30Hz 10 48K 1.5
5. Sensor 3 (SNS) Processed Images 640x480x1 30Hz 10 48K 1.5
6. Monitor Images (with symbols) 640x480x1 30Hz 10 48K 1.5

Regards,

Ran

  • Hi ,

    Is the video decoder the right device you are looking for?

    TVP5158's input should be CVBS, and it outputs BT656 .

    But the image sensor should already gives BT656 or similar ports.

    Are you looking for CPU which can connect multiple image sensors ?

    BR,

    Eason