Other Parts Discussed in Thread: ADS1299
Hi
We are using 3 x ADS1299 for capturing EEG and ECG signal.
I have to know how i can effectively use the SRB1 and SRB2 in multi devices,we are configured the ADS1299 in diasy chanin mode.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ADS1299
Hi
We are using 3 x ADS1299 for capturing EEG and ECG signal.
I have to know how i can effectively use the SRB1 and SRB2 in multi devices,we are configured the ADS1299 in diasy chanin mode.
Hello Brian
We are giving common reference from forehead for EEG and given to all non inverting pins of the channels.
Right now we are not planning to give SRB1 and SRB2.
I want to know whether it is make a problem in my circuit.
Hello Brian,
Thank you for your support......
Also i have shared a single oscillator for three ADS1299 devices.
In this case what are the points i look into it, is it able to drive a single oscillator these three devices.
May i have to take care in the routing side ?
Hi Brian
Thank you for replay...
I will take care the clock drive capability in my design.
I have one more question regarding the multiple device in daisy chain configuration.
We configured three devices in daisy chain and that time it is challenging to meet the proper setup and hold for all devices.
The more devices in the chain, the more challenging it could become to adhere to setup and hold times. A star-pattern connection of SCLK to all devices, minimizing DOUT length, and other printed circuit board (PCB) layout techniques helps. Placing delay circuits (such as buffers) between DOUT and DAISY_IN are ways to mitigate this challenge.One other option is to insert a D flip-flop between DOUT and DAISY_IN clocked on an inverted SCLK .
Above paragraph i copied from the datasheet page number 34.
Is it mandatory add d flip-flop between dout and daisy in .Can i achieve the setup and hold time by proper placement and software.
Please give me your suggestion on this case.
Hi Brian
Hope you are doing well.....
I have one doubt regarding the bias configuration in multiple devices.
In our multiple device diasy chain configuration
BIAS REF pin from three devices connected together and gave option for external reference.
BIAS INV pins from three devices connected together.Also each BIAS INV pin connected to the BIAS OUT pin of same device through external filter.
BIAS IN pin of all the device connected to the BIAS OUT of corresponding IC.
And BIAS OUT from one device connected to the RLD of ECG and EEG connectors.
Is this configuration of BIAS is correct ?
Hi Biran,
Hope you are doing well...............
Last time i discussed you we have project with 3 ADS1299 chip connected daisy chain for EEG and ECG acquisition.
We received the board and tested internally.Now we sent 3 boards to customer.
My customer need electrode impedance measurement .
I tried to connect resistor in range 8K to the channel my input is single ended.And tried to capture the voltage by setting L_OFF register and Config4 register.But i couldn't read the value.You have any suggestion.