Hi,
I have to measure the ECG and respiration using only 2 leads without RLD out lead.
I am modifying schematic page from page no.58 of datasheet of ADS1292R.
1. Can I connect RLD_out to R4 and R6 instead of AVDD and remove R3 and R5.
2. I am connecting LA and RA to RLD_out through 10 MOhm resistor to improve CMRR as I dont have RLD out lead.
3. Can I put 51K resistor between C1 and IN1P and same for negative channel for patient protection.
4. Can I use DC lead off detection? As respiration channel has capacitors so is it possible to use DC lead off detection?
Thanks and regards,
Vishal