Other Parts Discussed in Thread: DAC8760
please check out this schematic that i edited based off of the schematic from http://www.ti.com/lit/df/tidr346/tidr346.pdf all I want is to be able to output + or - 5V (and maybe +-10v) commanded from a micro controller via serial control, I don't need the current output; so is it okay if i just disregard the current output pin? I changed the supply from +/- 15V to +/- 12V and I removed some caps from between, the now, -12V and AVss because that is how the datasheet showed it. do I need to connect TPAD to Avss? if this Schematic will not work would you mind giving me some guidance?