Other Parts Discussed in Thread: ADS1299
I’m trying to evaluate the ADS1299 for use in an EEG application using the EVM-PDK. Although EEG signals are in the range of 1-20uV, the particular type of EEG signal of interest in my project is actually sub-1uV, making results even worse.
The datasheet gives an equation for ADC resolution vs VREF which implies
LSB = 539nV for VREF=4.5V (internal reference)
LSB = 298nV for VREF=2.5V (external REF5025 2.5V reference)
If the max PGA gain is 24 and EEG signals are in the range of 1-20uV then, without a preamplifier, the input of the ADC for EEG signals is 24-480 uV resulting in, according to my calcs, a range of:
44pk to 890 pk for VREF=4.5V (internal reference) ---- approx. 5-10 bits resolution
80pk to 1610 pk for VREF=2.5V (external REF5025 2.5V reference) ---- approx. 6-11 bits resolution
The first question is why isn’t a larger preamplifier gain included in the front end of an IC advertised as an EEG system solution?
The second question is how low can I set VREF to expand the conversion range? The external precision reference ckt in the datasheet shows the REEF5025 which is 2.5V but the Electrical Specs merely state both internal and external reference voltages as 4.5V typical.
No external preamplifier is mentioned in the applications docs or datasheet. Is there a recommended preamp device for EEG applications. It would seem that for my application, let’s call it 1uV pk-pk, I would need an overall gain when using a VREF of 2.5V of 2.5V/.000002V = 1.25M!!!! Given the PGA at x24 this still yields an external gain of 52,000.
Comments????
Jim