Other Parts Discussed in Thread: DAC3171
Customer is using DAC3171 and trying to use 7-bit interface mode.When they read config6:bits 7-0, the read 0x90 which indicates only 14-bit interface mode is supported. They are clearing config1:bit13 to tr yto put the device in 7-bit interface mode.
Why are they not reading 0x10 from config6:bits7-0 (they read 0x90)? Can they do anything to change what value they read here?
Are there DAC3171 devices that only support 14-bit interface mode and not 7-bit interface mode?
We are using datasheet SLAS959A.
The markings on the device are:
DAC3171I
TI 33J
P3D6 G4