This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1274 Low Frequency Noise

Other Parts Discussed in Thread: ADS1274

ADS1274 - What is the noise from 0.1H - 10Hz, expressed in uVp-p at the ADC input? This spec. is common forTI low noise OpAmps, etc.

  • Hi Ronald,

    Noise in uVpp can be taken from 1-sigma deviation from the mean of the histograms in Figures 4, 8, 12, and 16. The uVrms value specified in the datasheet is equal to uVpp / sqrt(2). These plots were recorded with the ADC inputs shorted together and biased to mid-supply. The noise specs will hold true for the maximum data rates listed in Table 2 for each operating mode.

    Best Regards,