This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Script files for adc08d1520rb

Other Parts Discussed in Thread: ADC10D1000, WAVEVISION5

Hi,

Which cpp script files are used for the adc08d1520rb? I could not find anything bearing the name of the ADC.

Regards,

Supratim

  • Hi Supratim

    Two different types of script files are used with Wavevision 5, ones with .cpp suffix as you mentioned, as well as ones with .xml suffix.

    The ADC08D1520RB uses a .xml script file. The full name of the file you are looking for is:

    "adc10d1000_xc4vlx25_adc08d1520rb.reg.xml"

    You should be able to find it in the following folder location:

    C:\Program Files (x86)\National Semiconductor\WaveVision5\hardware\scripts

    Best regards,

    Jim B