Hello,
I am using the ADC12J4000EVM together with the TSW14J56 Rev B EVM board. The Software I use is the ADC12J4000EVM GUI V1.3 and the HSDC Pro V3,0.
I use the On-board clock source with Fs = 3760 Msps. In Bypass Mode everything works fine. Also in Decimate-by-10; DDR and Decimate-by-20; SDR I am able to capture the single tone I am generating with a signal generator.
But if I try Decimate-by-4; DDR or Decimate-by-8; DDR/SDR (with and without the P54 option) it doesn´t work. I always get the Error "Read DDR to file TIMED_OUT_ERROR Time Out error".
Thanks,
Markus