We need to exploit a data acquisition system of 15 channels , the isolation voltage between these channels is greater than 100V and less than 2000V, the sampling rate is 500Hz. The iso7341c is used to isolat between these channels ,then comunicate to the arm.
1、we download the ADCPro Launcher "adcpro-wlvrt-2.0.1.exe"and "ads1281-adcproplugin-2.0.0.exe",after installing,the interface of the sofeware is"DSP not ready";
if we need to have an external +/-10V and 6V connected to the EVM/motherboard ;
how to connect the pins of the power ;
2、Please provide the diagram of the MMB0 board ;
3、Please provide the software program of the TMS320VC5509APGE in the MMB0;
4、If the other motherboard(similar to MMB0) can match ADS1281EVM ;
5、please point out the position of SPI interface of the MMB0 which can link to arm;