Other Parts Discussed in Thread: AFE4490SPO2EVM, AFE4490
Hello,
We have prepared a PCB of AFE4490SPO2EVM as per the reference design in user guide for evaluation purpose.
Currently PCB hardware testing is going on without loading the actual firmware. Few test programs for testing the MSP430 Functionality were loaded and they worked . But didn't tested AFE4490 functionality in hardware or firmware means.
After populating components while we testing the voltages in the circuit it is found that the the output of the diodes D1, D2, D3 and D4 is showing as zero volt.
In my understanding the power circuit are working properly and the input to the diode are proper ie Rx_ANA_SUP (3 V) & LED_DRV_SUP(5 V) are coming between the second and first (GND) pins of each diodes. But the voltage between the pin 3 of each diode to the and GND is showing as 0V.
While I measuring voltage at a EVM purchased from TI, it showing voltages at 3 rd pins of D1 & D2 as 0.88 V and at 3 rd pins of D3 & D4 as 2.35 V. Only difference this board and our board is firmware is not loaded.
I have checked after replacing the diodes(So I think it is not the issue of diodes also all of the diodes showing same result) and after removing the jumper resistors R24(INM), R27 (INP), R44(TXM) & R48(TXP) lines to isolate connection to the AFE4490 chip to the diode. But the results were same.
With these data can we assume any issue in our circuit? if so how can we trace it?
Please provide the normal voltage ranges needed to get at the 3 rd pins D1, D2, D3 and D4 pins in different conditions in normal connection and while isolated there connection to the corresponding pins AFE4490 ( ie removing jumper resistors R24, R27, R44, R47).
My assumption is that the issue happen due to AFE4490 chip side connection. Is any relation with these voltages with firmware?
Also, kindly request to provide suggestions for overall testing and troubleshooting the AFE4490 related circuits of the AFE4490SPO2EVM board