This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unipolar vs. bipolar ECG measurement circuits

Expert 1110 points

Hi team,

I have a very basic question. Consider that I have three electrodes. In one case I want to make a bipolar measurement (like between electrode 1 and 2, and between electrode 3 and 2). And in another case I want to measure a unipolar signal considering the electrode 2 as reference. How the circuit for these approaches are different? Is there any difference even? I know that in the first case I can connect the electrodes to the inputs of two in-amps. In this case electrode 2 would be connected to both in-amps. Please answer considering two options, with and without Right Leg Drive.

Appreciate any help.