Forking this post into it's own thread.. Here's the recap
Jon Mundall Wrote:
On another note we had issues with our ADS131e08's burning out when over saturating the inputs while running at a high gain, current was limited to 1/10'th of the data sheets recommendation but this appears to be invalid when using the PGA, please design accordingly or if anyone has ideas why this is happening please let me know.
The Ads131e08 is still by far the best part out there and were still using it on all our new stuff but it would be nice If it was a bit tougher or at least had documented behavior
Jon
would you be willing to share with us (TI) under which conditions you experienced damage to the ADS130E08 (maybe in a separate post)? We would like to understand that in more detail.
As long as you limit the input currents to save levels there should no damage occur to the device. The PGA should have no influence here.
Regards,
Joachim Würker
Systems & Applications Manager
Precision Delta Sigma ADC's
@Joachim,
This was our setup when we experienced the ic failure.
Power Supply is 2.4V Bipolar
Chip failure occurred when a gain of 12 was used and 12V test supply was applied to both inputs terminals.. 12v through a 25K resistor should limit the current to 0.48ma, there was also diodes to protect in case of a surge as shown in the below schematic.
It is also worth noting that the entire chip failed and would no longer return it's ID via SPI
When testing the failure did not happen immediate although we did notice it was causing a drift in the other 7 channels consistently
Further testing has not been performed beyond verification of digital voltage supply (3.3V) and analog supply (+/- 2.4V)