This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4300 Calibration pins: resistors & capacitors

Other Parts Discussed in Thread: AFE4300

Hello,

Will the AFE4300 work if I do not use the four 10M resistors connected between pins 28-31 you have in the tidra02 reference design available on your website? 

The AFE4300 documentation says nothing about these resistors.

These pins are intended for calibration of the chip and they do not come into contact with the patient. Thus, I want to remove the capacitors you have connected there as well (the 1uF C27-30 and the 0.1uF C5-8 capacitors in tidra02).

Will that be a problem?

Please let me know.

Thank you,

Mastro.