Sir
We plan to use LM98640 to process Infra-Red detector output which is 2V range with 2V of fixed offset. Fixed offset of 2V needs to be subtracted from signal. We plan to do it externally using OSx+ and OS- pins. If you refer Figure 10 on page 26 of datasheet, Csh capacitor can remove fixed offset voltage. Please, tell me can 98640 input take 4V maximum when other input is at 2V fixed level ? After differential input going to capacitor, fixed voltage will get cancelled out. In this case, can input be more than 2.85V specified in datasheet ? What is CMRR of first stage ? We need 14 bits digitization to cover large dynamic range of infra-red camera. Please, reply.