Hi,
we would like to use the ADC16V160 for mass production, but we have problems to verify the ENOBs on the eval board. We would appreciate if you can help us with our problem.
TI’s webpage says that the ADC16V160 has an ENOB of 12.3.
The datasheet (Fig. 10) says, that the SINAD @40 MHz is 77, which is 12.49 ENOB.
We have the eval board HFEB and we directly couple 160MHz into the device using an SMD oscillator.
Table 1, ENOB over VPP dependency
VPP [V] |
0,1 |
0,3 |
0,5 |
0,7 |
0,9 |
1,1 |
1,3 |
1,5 |
ENOB Tektronix |
11,132125 |
11,017 |
10,77725 |
10,631 |
10,010625 |
9,674875 |
9,042125 |
7,60987375 |
ENOB Agilent |
11,605625 |
10,64325 |
9,87825 |
8,98225 |
8,97 |
7,8625 |
7,8325 |
7,89175 |
We use an arbitrary function generator from Tektronix (AFG3102) and one from Agilent (3325DA) to generate a 40MHz sinus signal. We see an ENOB over VPP dependency (Figure 1) using WaveVision 5 for on the fly ENOB calculation. The ENOB is very low for a realistic VPP of 1.5V and even at a VPP of 0.1 V, we cannot reach the 12+ ENOBs from the spec.
Please let us know, if the ENOB over VPP dependency is realistic, or if anything is wrong in the setup we use.
Please advice, how the ENOBs can be improved in the Setup and how an ENOB of 12+ can be verified on the eval board.
Thanks a lot for helping and your advice,
Best Regards, Florian