Dear forum,
We have some cases of the TVP5150AM1 failing to reset properly. The problem is intermittent and only happens on some boards. In an attempt to fix the problem, we pulled the RESETB pin to ground through a 10k resistor. According to the data sheet, the input current should be +/-20uA so I expected to see RESETB float up to less that 200mV. Instead, it floats up to 1.2V impying an input current of -120uA. I thought this indicated a degraded device, but TVP5150AM1 devices which do not exhibit the intermittent reset failure problem also seem to have input current on the RESETB pin of 120uA, six times the value in the data sheet. For the test, the reset pin was connected to an Altera Cyclone III in tristate mode. Do you think this behaviour is normal?
Yours sincerely
Stephen Blake