Other Parts Discussed in Thread: ADS1015, ADS1115
My customer wants to use this part for current sensing. They will be using it in Differential mode, with the two inputs of the ADC connected to the two side of a small resistor (say 2 Ohms), and then use the internal amplifier to increase the signal level so as to maximize the usage of the DAC. Please confirm this part is ok with this kind of application?