Hi,
On page 26 of the datasheet for the ADS1278, Table 7, a clock frequency range is given for a certain DVDD. The language indicates this is only for maximum data rate but the table seems to indicate that this is the only valid frequency range for a given DVDD. Can you use a DVDD of 2.1V and a clock slower than 32.768 MHz (with a lower data rate)? The language indicates you could drop all the way down to 100 kHz with a DVDD of 2.1V. Is this correct?
Thanks,
DJ