I'm trying for some time to communicate with the ADS1018 but I can not seem to get any data back.
1st of all I've verified all connections to the device with a DMM and checked for voltages. Everything seems to be 100% correct.
2nd, I've hooked up a scope to check if SCK is low while CS goes low. I also checked the data on the falling SCK edge using a scope and it was as expected. What could be the reason the DOUT pin is set high (1) all the time?