Other Parts Discussed in Thread: ADS5401
I'd like to verify my understanding of the ADS5401 interleaved ADC pair's operation. I've read through the ADS5401 data sheet (SLAS946A - APRIL 2013 - REVISED JANUARY 2014), and, from the diagram on p. 24, I see that the interleaved ADCs operate 180 degrees out-of-phase from each other. I interpret this to mean that one of the ADCs samples on rising edge of the Fs/2 clock, while the other samples on the falling edge. If this is correct, I would expect the ADS5401's DA[11:0]P/N output to always begin with the output from the same interleaved ADC. Is that correct?
In other words, let's suppose the two (physical) ADS5401 interleaved ADCs are named "ADC A" and "ADC B". After power up, the DA[11:0]P/N output will then alternate between data samples digitized by ADC A and by ADC B. Is it true though that the first ADC sample on the data lines always comes from, say, ADC A? Or does the ADS5401 output sometimes start with ADC A's data and, at other times, with ADC B's data? If the former is correct, I'd like to confirm that I could collect the even- and odd-numbered ADS5401 samples from data collected under different conditions (e.g., after multiple power-cycles, hardware resets, etc.) and be assured that each sample set is data from the same (physical) interleaved ADC.
Thank you in advance for any help in understanding the interleaved ADC operation.