This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12J4000 Lane rate

Other Parts Discussed in Thread: ADC12J4000

Hi

My cutomer is using ADC12J4000.
He wants to use with the following condition.
Is this possible?

- Device clock : 3.6GHz
- 8 lanes output
- M=8 S=5 N'=12
- Not decimation (law data use at FPGA)

Could you let me know the calculation formula for lane rate?

Best regards
Shimizu

  • Hi Shimuzu

    The easiest way to find the output lane rates is to look at Table 11 in the ADC12J4000 datasheet. The device has fixed output rates specific to each Decimation factor setting, as well as the formatting. The available rates are 1x, 1.25x, 2x and 2.5x the input DEVCLK frequency. 

    For No Decimation, the output lane rate is always at 2x the ADC device clock frequency, so in this case the rate would be:

    2 x 3.6 GHz = 7.2 Gbit/sec on each of the 8 lanes.

    The calculations for each mode can be fairly complicated, especially for those modes where Tail bits are added to optimize the link data rate to match the available output rates.

    Best regards,

    Jim B

  • Hi Jim

     Thank you for your support.

      I understood

    Thanks

    Shimizu