This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can I use DAC2932 statically? Does DAC2932 have a required minimum clock frequency?

Other Parts Discussed in Thread: DAC2932, DAC2932EVM

Dear all,

I'm reading the datasheet of DAC2932, which is a "dual, 12-bit, 40MSPS, Digital-to-Analog Converter". 

In "Timing Requirements I-DAC" on Page 6, the parameter tCP (Clock cycle time (period)) has a typical value of 25ns, which translates to a frequency of 40MSPS. It does not specify a maximum tCP (or a minimum clock frequency).

I'm just wondering, if I can use this DAC statically. I mean, if I can latch the parallel data input [D11:D0] only once, and have the DAC retain the current ever since without feeding it a clock to update the parallel data input?

Essentially it will depend on how the latch is implemented in the DAC. If it is a dynamic latch, it will need constant update, otherwise the data will fade. If it is a static latch, even without being refreshed, the data will retain, hence the output current too.

The datasheet is available here: http://www.ti.com/lit/ds/symlink/dac2932.pdf

I'll be extremely grateful if you can answer my question. Thank you!

BR,