Dear all,
I'm working on an application in which I will use only 5 electrodes ( 2 for IN1, 2 for IN2, and 1 from the RLD).
However, I'm not sure how to bias IN3P and IN3N if I'm not going to use them. Should I ground them or pull them up to VDD by means of a pull-up/pull-down resistor? or are there other uses of it? (I saw that you can time multiplex IN3 with IN2 or IN1, but it's probably not convenient in my case as I really need the EMI filters in the input).
Also, are these IN3 inputs included in all the ADS1292 versions? or only in the ADS1292R one?