This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DDC11xEVM-PDK

Other Parts Discussed in Thread: DDC11XEVM-PDK, DDC114, DDC112

Hi,

It is a question for the set of DDC11xEVM-PDK.

When you purchase a DDC11xEVM-PDK, do you have two of EVM of DDC112EVM and DDC114EVM is enclosed?

Do you need to purchase separately?

Best regards

  • Cafain-San,

    The DDC11xEVM-PDK kit contains: one DDC112 daughterboard, one DDC114 daughterboard, and one USB motherboard. All three boards are contained in one kit, there is no need to buy them separately. Either the DDC112 daughterboard can be used or the DDC114 daughterboard can be used, they cannot be both used at the same time. Both of them use the same USB motherboard.

    Regards,

    -Adam Sidelsky