Other Parts Discussed in Thread: ADS1255, ADS1256
Hii,
I am using ADS1255 ADC. the problem is that when i give input to AIN0 when buffer is on it will give reading upto 2.1V.but when buffer is off input range is 3.0V. means when i off the buffer ADC count is decreased for same input.
my reference is 1.2 V. and i use ADC in 18 bits but it should give count to only 244k instead of 262K.
Please provide suggestions.