Other Parts Discussed in Thread: ADC12D1800
Hello,
I am using a ADC12D1800 on a FMC161 mezzanine by 4DSP with a VC707 motherboard by Xilinx. The ADC provides clock and data to the motherboard Virtex 7 through a FMC connector.
I provide the ADC with a 910MHz clock; it should forward a 227.5 MHz clock to the Virtex 7. The FPGA MMCM successfully locks unto the clock, never looses lock and the MMCM divide-by-1 output clock on a SMA test point is at 227.5 MHz. So far, so good.
I believe I successfully command the ADC to go to test pattern since I do see the test data on my pins when I request it. However, the pattern is stuttered. I see : 0004000000100008 six times in a row, followed by 0ffb0fff0fef0ff7 four times in a row. This pattern always repeat.
I am at a loss. Any idea?
Thank you,
C Gyselinck