Other Parts Discussed in Thread: ADS1292R, ADS1292
Hi. I had configured ADS1292R to generate the test signal and have displayed square wave at 1 Hz, so communication with the microcontroller is correct. I try to measure ECG using only 2 leads without RLD out lead, but a get wrong data.
My ADS1292R configuration is:
ads1292_Reg_Write(ADS1292_REG_CONFIG1, 0x00);
ads1292_Reg_Write(ADS1292_REG_CONFIG2, 0xA0);
ads1292_Reg_Write(ADS1292_REG_LOFF, 0x10);
ads1292_Reg_Write(ADS1292_REG_CH1SET, 0x80);
ads1292_Reg_Write(ADS1292_REG_CH2SET, 0x40);
ads1292_Reg_Write(ADS1292_REG_RLDSENS, 0x00);
ads1292_Reg_Write(ADS1292_REG_LOFFSENS, 0x00);
ads1292_Reg_Write(ADS1292_REG_RESP1, 0x00);
ads1292_Reg_Write(ADS1292_REG_RESP2, 0x00);
ads1292_Reg_Read(ADS1292_REG_RESP2, 0x00);
I'm confused, can anyone help me?
Regards,
Victor