Hi to all,
I was using the ads1100 as single ended to measure and input from 0 to 5V max. Now I have to measure 4 inputs in the range of 0 to 5V (single ended app). I was looking at the ads1115 to perform this task, but I have a few questions:
1) To reach the 5V FS I have to set the PGA reg to 0 (2/3 gain), in this case what is the value of the voltage reference?
3) the output code will be 32768 for the 5V input or the value of the voltage reference?
regards
Gastón