Hi Jim,
Another question about the ADS54J60...My signal of interest falls in the 2nd Nyquist and I have researched the setup in the datasheet on pg. 43. I have set 0x68004E to 0x80 and 0x6800042 to 0x01. Further, following the board schematic and layout files, I have bypassed the ADT1-1WT and am using a more appropriate balun.
This issue, is that I got great performance improvement using the 2nd Nyquist IL correction on two different occasions, but I am now not able to get the same result. Even though the said registers read back the correct IL correction values mentioned above, the performance is not reflecting the same data taken with the correction was seemingly turned on.
For example, at 750MHz the SNR (before vs. after) is 62.95dB and 31.57dB.
Do you have any performance data available that were taken in the 2nd Nyquist?
Also, is there a specific SPI write sequence that I should follow to implement the IL correction?
Lastly is the performance increase that I have seen possibly due to some other artifact of the HSDC Pro software?
Thanks,
Justin