Been using WaveVision for a while now - good program.
However, today it's developed a bug. When importing ASCII decimal data, it's impossible to enter a value in the "Sample Rate:" box; it remains blank, and does not respond to typing in digits. However the Sample Width can be adjusted.
Consequently, calculations that use the sample rate, such as an FFT, cause a crash and bring up a "Report and Suggestion Editor". The report contains "Exception Message - Scrollbar Property Out Of Range", which makes sense as the frequency axis values displayed are garbage. But, I can't enter a name or email in the report dialog, though there is a correct email present in report's the "General" tab. But on trying to send it, there's an "unexpected error prevented the message from being sent".
Uninstall & reinstall did not fix it.
Any help with getting round this issue is appreciated.