Other Parts Discussed in Thread: ADS1274
Hello, I am using ADS1274 in my sensor interface module.
I think the nDRDY of ADS1274 should be changed periodically if powers(DVDD,IOVDD,AVDD) are properly provided to the ADC and if CLK is also properly provided,
but I found one problem in my sensor interface module.
When I turn power supply, sometimes nDRDY of ADC is not changed periodically and just it remains high.
In this case, If I do pwer-cycle(turn-off and on again), nDRDY starts work correctly.
CLK is always provided correctly in all cases.
In my sensor interface module
DVDD=1.8V
IOVDD=3.3V
AVDD=5V
and 5V AVDD is LDO regulator(TPS70950) output (7V input)
and 3.3V IOVDD is LDO regulator(TPS70933) output (5V AVDD input)
and 1.8V DVDDD is LDO regulator(TPS70918) output(3.3V IOVDD input)
so, consequently, AVDD is the first applied, IOVDD is the next applied , and DVDD is the last applied.
Is there any requirement of power up sequence or power rising time requirement? or any other?
Please let me know your valuable recommendations/opinions about this issue.
Best Regads
Hak-Jin Jeong