I plan to use your ADS1018, I want to operate it down to about 2.1V, using it in single ended mode. But I want to get the full 12 bit range of 0-4095 so what would the PGA need to be set to? I can use an input range of 0-1.024 or 0-2.048. If I can't get the full range with this part can you recommend a different part. I need a 4 channel single ended device, 0-70V, operate down to ~2.1V, SPI interface, 12 bit. Thanks