Other Parts Discussed in Thread: THS770012, ADC16V130
Hi,
I am using THS770012 to drive ADC16v130 with a band pass (IF 70MHz and BW of 16MHz) filter between them.I am using 50ohms series termination at THS output and 100ohms differential filter.But a am not able to get 2.5Vp-p swing at ADC input it was around 800mVp-p.PCB layout has no issue, simulated and tested.Please suggest the interfacing circuit.I am attaching the screenshot of the portion of relevant circuit for reference in a zip file. THS770012.zip