Other Parts Discussed in Thread: ADS1298, ADS1299, ADS1198
Hi,
I'm looking to daisy chain two TI ads1298 or 99 boards and interface them to the computer via USB through an arduino due and adafruit usb isolator

which maxes out at 12 Mbps.
I'm confused as to how I can determine if the transfer rate (12 Mbps) is high enough for my purposes. I'm looking to stream data from 16 channels at up to 2000 sps at let's say a 24 bit precision, though 16 may be enough.
Thanks!
-David