Other Parts Discussed in Thread: ADS1293EVM, ADS1293
I am planning to use ADS1293EVM and stream its output via a Bluetooth device for a demo project. I see that ADS1293EVM has an SPI jumper to probe the SPI pins of the chip. Is it possible to initialize the ADS1293 chip through this SPI probe interface?? I want to collect the output from ADS1293EVM and directly connect it to bluetooth board, instead of reading the EVM output to PC via the USB port. Any help is appreciated.