Hi,
I don't know what happened, but I can't configure the DAC3484 EVM via the GUI. If I try, for example to enable an option, it goes immediately back disable or if I want to setup the Input Format to "2's complement", it goes back to "offset binary". The GUI doesn't write any of my setups except the CDCE62005 setups. It is strange...Is my EVM defect?
Thanks a lot.