Hi,
ADC3222 Front-end Circuit(Opeamp)
1) Although analog input is ± 1V = 2Vpp, does it can be used in single-ended.
If possible, please tell me the circuit configuration.
2) In the data sheet, and to change the analog signal of single to differential, it's using a transformer,
We want to achieve an operational amplifier.
Please tell me the optimal device name. Further, the circuit does it also can suggest?
Best regards