Other Parts Discussed in Thread: ADS1298
Hi,
I am trying to make the ads1298 evaluation board to work with active electrodes.
I try to do that for an emg application so I bypass the dummy connector and connect the 2 differential signals of the electrodes on JP33.
For the DRL I'm using a passive electrode and I connect it on JP1 on the side of DRLOUT.
I supply the buffers of the electrodes from a 5V TP and a ground TP from the board.
When I connect the board to the power supply and before connect the active electrodes to their power supply from TP there are some LEDs that turn on. When I, subsequently, connect the TPs to the electrodes' supply, the LEDs turn off and the board doesn't seem to work.
Do you see any problem with these connections?