Hello,
I am designing an automated measurement & characterization system for various resistive sensors and the DAC8760 seems to be an ideal choice for the application since it can provide a current output with suitable voltage compliance and a variable voltage output which might be useful for additional functions.
The sensors I have to test display a resistance between approx. 50 Ohms and 60 kOhms, depending on the sensor type.
The low resistance sensors require a max test current of approx 22mA, the high resistance sensors require a test current around 500uA and there is also a third type with intermediate characteristics. Therefore as you understand I will need to cover a broad range of required current and voltage.
If you could provide some further details and recommendations to the questions below it would be very helpful.
1) Are there any limitations concerning the load impedance? Will it work ok for my application? As far as I saw the datasheet specifications are based on 300 Ohm loads only. Could you provide some data for the current output as a function of the load impedance?
2) I suppose it would be preferable to use both an external Rset and a boost transistor for my case since I will probably have a very large power dissipation on the IC otherwise. Are there any specific NPN transistors that you would recommend as a pass element?
Perhaps you could also provide some hints to improve the response and minimize offsets and stability issues due to the external transistor?
3) I would like to insert a low value (10Ohms) external sense resistor to measure the current applied. Would you recommend a differential/instrumentation amplifier or would it be better to use a chopper amplifier in order to minimize errors across the current range?
If you can suggest some suitable parts and an optimized schematic it would of course be appreciated.
4) I would like to alternate between connecting the current output and the voltage output of the DAC8760 to the device under test. It will not be required to change with a high frequency, only when the system initializes.
Do you think it would be preferable to implement this using a changeover relay or using 2 discrete JFETs or some other way in order to minimize noise etc?
Thank you for your time!