This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS131E08 REFERENCE

Other Parts Discussed in Thread: ADS131E08EVM-PDK

Hi,

I am using bipolar scheme which connects AVDD to +2.5V and AVSS to -2.5V and DVDD to 3.3V. I am confused by the reference connection.

According to the spec, looks like we connect VREFP to GND and connect VREFN to -2.5V, this way I believe we use internal 2.4V reference;

But if I want to use REF5025 for external 2.5V, the spec says VREFP max limit is AVDD which is +2.5V, so it is not good to connect it to VREFP. How should we connect the external reference if we want to use it? Or in this situation we only choose internal reference?

I definitely need help on this.

Thanks and best regards,

Qi

  • Hello Qi -
    You can reference the EVM schematic in the ADS131E08EVM-PDK on page 37 for clarification on the reference connection. An external reference is shown, U2 or U3 (along with the buffer), as an example. VREFN should always be AVSS. VREFP will be the reference voltage which will be referenced to AVSS.
  • Hi Greg,

    Thanks for the quick reply! I studied the page37 before but I still have concern.

    if I connect VREFN to -2.5V (AVSS), VREFP to +2.5V reference, then Vref = (VREFP-VREFN) = 5V which exceeds AVDD 2.5V specified by in page 3 of the spec.

    Best regards,

    Qi
  • Hello Qi -
    If you connect the reference IC with respect to AVSS and AVSS is -2.5V, for a reference IC that generates 2.5V, as long as you connect VREFP to reference output and VREFN to AVSS you will get VREF = 2.5V. VREF = VREFP=VREFN, where VREFP = ~0V and AVSS = -2.5V.