I am makeing a project using ADS1220 for full bridge measurement with ratiometric reference. 5V at the analog side and 3.3V at the MCU side ( a Cortex M0). I am using the ADS1220EVM as a reference design, but i could not get the function of the SPI buffers with the SN74LVC125. Any comments on that? Any reason i can see for that would to use an external SPI to control the ADS1220.
Regards,
Luis