I have one question about the 24bit ADC ADS1259 evaluation board. I plan to use it to measure the output of my DAC. However, my DAC output is from -5 V to 0 V, the ADS 1259 working is from 0 to 5 V. So can I use this evaluation board to measure my DAC? Is there any problem in hardware or software? thanks a lot!