Dear sir,
I was using DAC4814 ,I had faced many problem its not responding as mentioned in datasheets.So can I use DAC7714U IC in place of DAC4814.DAC7714 will be OK.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear sir,
I was using DAC4814 ,I had faced many problem its not responding as mentioned in datasheets.So can I use DAC7714U IC in place of DAC4814.DAC7714 will be OK.
1. i have +-12V,+-5V supply,I have to use as bipolar and alreay I have PCB where i was using DAC4814 but unfortunately DAC4814AP is not working and iam not getting anywhere so if we have same pin discription then it ill be good for my design.
2. And if we follow DAC7714 datasheet its written +-15V,so i have doudt i can use DAC7714 with +-12V.
3. Do you have embedded C code for the same DAC7714.