Other Parts Discussed in Thread: DAC9881, DAC7311, DAC8311
Dear Sir,
we are looking for a DAC converter which output range would be 0~10mV.
Could you please give me some suggestion? wich DAC of TI is siutable for our application? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Passerby,
Can you share a little more information about your application?
How many steps do you need from 0 to 10 mV? (Resolution)
What kind of of accuracy do you need at each step?
What are you trying to control with such a small output range?
Are you just trying to generate 11steps? 0 V, 1 mV, 2 mV... 9mV & 10mV? The DAC9881 it cannot do this on its own because of its large zero code error. It will require a negative supply and an external circuit to achieve this.
I would suggest taking a look at the DAC7311 and DAC8311 they have an extremely low zero code error of 0.2 mV typical and should also be able to meet your 1mV per step requirement.