Other Parts Discussed in Thread: ADS1292, ADS1292R
Hi.
We are trying to use an ADS1292 for vital signals aquisition.
At the moment there are a few problems we are facing without explanation or solutiuon, hence, I'm asking for some guidance here today.
1st: We have very good signal reading from the ADS from 125sps until 500, as soon as we select 1ksps, the signal arrives full of spikes. These happen +/- every 500ms. If we select 2Ksps then 250ms... etc
The code that makes the reading by the nREADY interrupt is the same for all the tries. Bellow 1Ksps works fine, above is spiky and noisy. The reading system could go up to 20ksps if needed.
2nd: Once our system is prepared for a 12bit sampling, we where hoping that a simple passage from 24 bits to 12 would be enough for signal reconditioning.
We observed that the signal was in fact falling on the right averages but a lot smaller, leading to the question, why isn't the signal being read at 24bit with the same magnitude when compared to a 12bit ADC, injected with the same source.
he config2 voltage is being left with the default of 2.42v ref.
2 leads only, there is no RLD setup. Design circuit is according to Figure 56, of page 58.
Avdd is 2.5V
Thank you very much for time and attention to our complications.
And thank you in advance for your reply and help.
-- Ricardo --