Other Parts Discussed in Thread: AFE7225
Will be clocking the AFE7225 using a single-ended LVTTL 60 MHz clock and enabling the single-ended buffers for DAC and ADC on chip.
Will connect coupling caps to pins 8 and 9 and then tie together (per data sheet) and feed from a single LVTTL clock.
Question: What is the acceptable level range when using the single-ended clock inputs? Can we drive them directly with LVTTL (3.3V) levels?
Thanks,
John