Hi,
I think there is an error with the numerical values in data sheet §9.4.7.3.3.1. Text is right and computation works as written. Just numerical values in example are wrong.
is there anyone to confirm ?
regards
Hervé
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I think there is an error with the numerical values in data sheet §9.4.7.3.3.1. Text is right and computation works as written. Just numerical values in example are wrong.
is there anyone to confirm ?
regards
Hervé
Hi Hervé,
You are correct! Adding 12h + 34h + 56h+ 78h + 9Bh should provide a checksum = AFh. I've made a note of the data sheet error. Thanks for the feedback!
FYI: There is an Excel Calculator that will provide you with the correct Checksum and CRC calculations for the ADS1262. It can be downloaded from:
(http://www.ti.com/lit/zip/sbac137)
Best Regards,
Chris