Hello,
I had a hard time following the .
I have followed "3 Basic Test Procedure with TSW1400" procedure from the DAC348x EVM user's guide exactly
but I get distorted signal definitely having spectrum not as I see in HSDC Pro.
The only subjective factor I can see is 1228.8 MHz at 1.5Vrms signal.
So I decided to use the internal 19.2 MHz oscillator.
I have loaded DAC3482_FDAC_1228p8MHz_4xint_NCO_30MHz_QMCon.txt and
then I have modified the registers of CDCE62005 into what I believe is equivalent (but for internal clock)
reg value
00 0x80400000
01 0x813C0321
02 0x81400302
03 0xC10C0303
04 0x00040304
05 0x28001A85
06 0x44AF0776
07 0x145294A7
08 0x20001C08
With this settings I seems to be closer but not exactly I get two energy bumps similar as I see in HSDC Pro
One at around 60MHz and another around 92MHz
Any help rectifying this?
In addition I wont to use the Multi tone Generator (initially for only one tone ).
Can someone point me to the settings I should use.
If I just try to create 1 tone at around 50MHz using the same DAC settings I get distorted signal.
Thanks
Dimitar